CMP#.REARM

Description

CMP#.ARM sets the automatic rearming behavior for the setpointClosedSetpoint is the target value that an automatic control system, for example PID controller, will aim to reach. It determines whether CMP#.ARM resets to 0 after a compare event, or stays set to 1 continuously. It may be changed while the compare channel is running and the setpoints are armed.

It takes two command line arguments: the first specifies the setpoint, and the second turns rearming on or off.

Examples

Usage

0: Disable rearming, enable single shot arming (default)

1: Enable rearming, enable continuous arming

Code

The following commands turn on rearming for setpoint 0 of channel 1, and turn off rearming for setpoint 4 of channel 2.

--> CMP1.ARM 0 1
--> CMP2.ARM 4 0

Context

For more information please refer to Compare.

Versions

Action Version Notes
Implemented 02-06-00-000  

General Information

Type

Read/Write

Units

N/A

Range

0 to 1

Default Value

0

Data Type

Integer

See Also

CMP#.ARM

Stored in Non Volatile Memory

Yes

Variants Supported

All variants are supported.