DRV.DIFVAR

Description

This parameter displays all parameters which have different values than their default setting. The actual value of each parameter is directly shown after the command name and the corresponding default value is then shown in brackets.

This command also shows differences in parameters which hold a string, such as AXIS#.NAME.

Example

-->DRV.DIFVAR

DRV.EMUEMODE 10 (0)

AXIS#.NAME MyDrive(no-name)

FB#.ENCRES 0(1024)

AXIS#.ILClosed"Instruction list" This is a low-level language and resembles assembly.KP 50.009(24.811)

AXIS#.PL.KP 99.998(49.999)

AXIS#.VL.KP 0.108(0.000)

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read Only

Units

N/A

Range

N/A

Default Value

N/A

Data Type

String

Stored in Non Volatile Memory

No

Variants Supported

All variants are supported.