DRV.REBOOT
Description
This parameter performs a software reboot when the following command is issued in the WorkBench terminal:
DRV.REBOOT 0xAABBCCDD
WorkBench will disconnect from the AKD2G when the reboot command is executed. The AKD2G can be reconnected to WorkBench approximately one minute after the reboot command is issued. The parameters stored in non-volatile memory will be restored to the AKD2G once rebooted.
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-00-00-000 |
General Information
Type |
Command |
Units |
N/A |
Range |
N/A |
Default Value |
N/A |
Data Type |
Integer |
Stored in Non Volatile Memory |
No |
Variants Supported
All variants are supported.