EEO#.MODE

Description

This keyword specifies the type of output waveform an EEO generator will create.

SOURCE    
0 (default) A Quad B
1 CW/CCW
2 Step/Direction

Examples

Code

This will set the 2nd EEO output mode to Clockwise/Counter-clockwise.

-->EEO2.MODE 1

Context

For more information see Encoder Emulation.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type Read/Write
Units N/A
Range 0 to 2
Default Value 0
Data Type Integer
See Also  
Stored in Non Volatile Memory Yes

Variants Supported

All variants are supported.