REC.OFF
Description
REC.OFF turns the recorder off. In order to set the recorder again, the recorder must first be armed and then a trigger set.
Examples
Code
If a recording is triggered before this command is executed, this command will cancel the recording and the recording state will go to Idle.
-->REC.OFF
Context
For more information see Scope.
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-00-00-000 |
General Information
Type |
Command |
Units |
N/A |
Range |
N/A |
Default Value |
N/A |
Data Type |
N/A |
See Also |
REC.ACTIVE, REC.DONE |
Stored in Non Volatile Memory |
No |
Variants Supported
All variants are supported.