VBUS.RMSLIMIT
Description
This parameter reads the limit of the bus capacitor AXIS#.LOAD. When the bus capacitor loads exceeds this limit, the drive generates fault F503.
Excessive bus capacitor load may indicate a disconnected main supply phase.
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-00-00-000 |
General Information
Type |
Read Only |
Units |
Vrmsrms stands for root mean square (also known as the quadratic mean) |
Range |
N/A |
Default Value |
N/A |
Data Type |
Integer |
See Also |
N/A |
Stored in Non Volatile Memory |
No |
Variants Supported
All variants are supported
Related Topics