VBUS.VALUE
Description
This parameter returns the measured DC bus voltage.
Examples
Usage
The DC bus voltage measurement is used to detect unsafe operating conditions and protect the drive power electronics.
Code
--> VBUS.VALUE
159.997 [Vdc]
Context
For more information on DC bus operation and protection, refer to Power View and Regeneration.
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-00-00-000 |
General Information
Type | Read Only |
Units | Vdc |
Range | N/A |
Default Value | N/A |
Data Type | Float |
See Also | VBUS.UVMODE |
Stored in Non Volatile Memory |
No |
Variants Supported
All variants are supported.