Motor Temperature View
The motor temperature settings are located in the nested Motor Temperature view.
Element | Description | Command |
---|---|---|
Thermal Resistor Type |
Select the type of thermal resistor.
|
AXIS#.MOTOR.RTYPE |
Thermal SensorA sensor is a type of transducer that converts one type of energy into another for various purposes including measurement or information transfer Source |
Set the source of the thermal sensorA sensor is a type of transducer that converts one type of energy into another for various purposes including measurement or information transfer. This indicates whether the thermal sensor is connected to the drive through a direct wire connection or through a digital feedback channel.
Devices with a feedback use AXIS#.MOTOR.RSOURCE, while sensorless motors (type 2 or 10) use AXIS#.MOTOR.TEMPSOURCE. |
AXIS#.MOTOR.RSOURCE or AXIS#.MOTOR.TEMPSOURCE |
Actual Thermistor Value | This field displays the motor temperature, which is represented as the resistance of the motor's PTC or NTC. | AXIS#.MOTOR.TEMP |
Fault Level |
This field is used to configure the motor temperature fault level as a resistance threshold of the motor thermal sensor. A zero value prevents temperature faults from being reported.
|
AXIS#.MOTOR.TEMPFAULT |
Warning Level |
This field is used to set the motor temperature warning level as a resistance threshold of the motor's PTC. A zero value prevents any warning from being created. |
AXIS#.MOTOR.TEMPWARN |
Actual Motor Temperature | If the motor has a thermistor with linear characteristics (AXIS#.MOTOR.RTYPE = 2 [KTY83-110], 3 [KTY84-130], 4 [PTC + KTY83-110], or 8 [PT1000]),), this field displays the measured motor temperature in degrees C. For other values of AXIS#.MOTOR.RTYPE this field is hidden. | AXIS#.MOTOR.TEMPC |