FBUS.PARAM1 TO FBUS.PARAM10

Description

FBUS.PARAM01 sets the baud rate for the CANbus. Supported baud rates are 125, 250, 500 and 1000 kBaud. On AKD-C

FBUS.PARAM01 sets and stores the EtherCATClosed***EtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs station alias for the ESC (EtherCAT slave controller) of string 2.

FBUS.PARAM02 switches the phase locked loop (PLL) for synchronized use: 0 = OFF, 1 = ON. FBUS.PARAM02 only works when FBUS.TYPE = 3 (CANopen).

FBUS.PARAM03 sets and stores the EtherCAT station alias for the ESC (EtherCAT slave controller). On AKD-C, FBUS.PARAM03 sets and stores the EtherCAT station alias for the ESC (EtherCAT slave controller) of string 1.

FBUS.PARAM04 switches the surveillance of SYNC-signals: 0 = OFF, 1 = ON.

FBUS.PARAM05 is used to configure some special behaviors of the DS402.

FBUS.PARAM06 - FBUS.PARAM10 are reserved.

 

FBUS.PARAM04 Additional Notes

FBUS.PARAM04 enables (1) or disables(0) the synchronization supervision of the CANClosed"Controller area network" CAN is a broadcast, differential serial bus standard developed for connecting electronic control units. Each node is able to send and receive messages, but not simultaneously or EtherCAT fieldbus.

Default values:

  • CAN: disabled (0)
  • EtherCAT: enabled (1)

The synchronization supervision is active when:

  • FBUS.PARAM04 = 1
  • The first CANopen Sync message or first EtherCAT frame was received.

FBUS.PARAM05 Additional Notes

Bit 0 configures the behavior of DS402 state machine in case of fault resets.

Bit 0

 

1

Faults can only be reset using DS402 controlword bit 7. 

0

The reset can also be done using Telnet or digital input and the DS402 state machine reflects this condition.

Bit 1

 

1

The state of the hardware enable does not change the state machine to state Operation enable.

0

If the state Operation enable or Switched on is active, it falls back to the state Switch on disabled, if the Hardware enable goes to 0.

Bit 2

 

1

WorkBench/Telnet cannot software enable the drive when CANopen/EtherCAT are operational.

0

WorkBench/Telnet can software enable the drive.


  • During commissioning this bit should be set to 1 to avoid influences to DS402 power stage state machine. The fieldbus should not be in operation to avoid influence to test functions of WorkBench.

Bit 3

 

1

DS402 - state machine is not influenced if the software enable is taken away using Telnet.

0

DS402 - state machine is influenced if the software enable is taken away using Telnet.

Bit 4

 

1

Scaling is done using special DS402 - objects (independent on units)

0

Scaling for position, velocity and acceleration objects is done using UNIT parameters.

Bit 5

(EtherCAT only)

1

FBUS.PARAM03 defines the station alias address if not 0. If FBUS.PARAM03 is set to 0, the address will be taken from rotary switches if they are not 0. The EtherCAT master has the ability to use the alias address selected by the drive or issue its own.

0

The rotary switches define the station alias address if not 0. If the rotary switches are set to 0, the address is taken from FBUS.PARAM03 instead, if it is not 0.

Bit 6

 

1

Bit 0 of parameter MT.CNTL (object 35B9 sub 0) can be accessed.

0

Bit 0 of parameter MT.CNTL (object 35B9 sub 0) is exclusively used for DS402 controlword.

Bit 7

1

All capture objects (0x20A0-0x20A3, 0x20A6, 0x20A7, 0x60BA to 0x60BD) are scaled as object 0x6063.

0

All capture objects (0x20A0-0x20A3, 0x20A6, 0x20A7, 0x60BA to 0x60BD) are scaled as object 0x6064.

Bit 8

1

DS402 - state Switched on means power stage disabled.

0

DS402 - state Switched on means power stage enabled.

Bit 9

1

SDO content of object 0x6063 is the same as PDOClosedPDO is a type of protocol frame used in some fieldbuses. A PDO contains one or more object dictionary entries, which define the application data transferred between devices. content.

0

SDO content of object 0x6063 depends on AKD unit parameters.

Bit 10

(Bit 10 is active only,
if Bit 8 is set)

1

State Switched on can be reached without the high-level voltage being active.

0

State Switched on can only be reached when the high-level voltage is active; otherwise the drive stays in Ready to switch on.

Bit 11

1

No emergency messages over CANopen are triggered when a drive warning occurs.

0

Emergency messages over CANopen are triggered when a drive warning occurs.

Bit 12

 

reserved

Bit 13

(EtherCAT only)

1

Downloaded parameter file is stored automatically to nonvolatile memory.

0

Downloaded parameter file is not stored automatically to nonvolatile memory.

Bit 14

1

If a warning occurs which limits a movement of the motor bit 11 in the DS402 statusword is additionally set to bit 7.

0

Only bit 7 is set when any warning occurs.

Bit 15

1

The bit 10 of the statusword (target reached) is set as a reaction to the halt bit (bit 8) of the controlword when the motor velocity is below CS.VTHRESH. It is also set when doing a Quickstop (using bit 2 of controlword) when using quick stop option code (0x605A) 5 or 6 and coming to standstill.

0

Bit 10 of the statusword is only set when the external setpointClosedSetpoint is the target value that an automatic control system, for example PID controller, will aim to reach value of a movement is reached, e.g., target position in profile position mode.

Bit 16

1

The hardware enable input decides if the transitions between Switch on disabled and Ready to switch on are taken.

0

The decision relies on the DS402 controlword.

General Information

Type

NV Parameter

Units

N/A

Range

See table below.

Default Value

See table below.

Data Type

Unsigned 32

See Also

CANbus Communication Manual, EtherCAT Communication Manual

Start Version

M_01-00-00-000

Parameter EtherCAT COE Range CANopen Range
FBUS.PARAM01

AKD-C: 0 to 65,535

Other AKDs: N/A

125; 250; 500; 1000
FBUS.PARAM02 0 to 1 0 to 1
FBUS.PARAM03 0 to 65,535 N/A
FBUS.PARAM04 0 to 1 0 to 1
FBUS.PARAM05 0 to 511 0 to 511
Parameter EtherCAT COE Default Value CANopen Default Value
FBUS.PARAM01

AKD-C: 0

Other AKDs: N/A

125

FBUS.PARAM02

1

0

FBUS.PARAM03

0

N/A

FBUS.PARAM04

1

0

FBUS.PARAM05

0

0

FieldbusClosedA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design Index/Subindex Object Start Version

EtherCAT COE and CANopen

/0

FBUS.PARAM01

/0

FBUS.PARAM06

M_01-00-00-000

/0

FBUS.PARAM02

/0

FBUS.PARAM07

/0

FBUS.PARAM03

/0

FBUS.PARAM08

/0

FBUS.PARAM04

/0

FBUS.PARAM09

/0

FBUS.PARAM05

/0

FBUS.PARAM10