ANY_TO_TIME
Inputs
IN : ANY Input value
Outputs
Q : TIME Value converted to time
Remarks
For BOOL input data types, the output is t#0 ms or t#1 ms. For DINT or REAL input data type, the output is the time represented by the input number as a number of milliseconds. For STRING inputs, the output is the time represented by the string, or t#0 ms if the string does not represent a valid time. In FFLD language, the conversion is executed only if the input rung (EN) is TRUE. The output rung (ENO) keeps the same value as the input rung. In IL"Instruction list" This is a low-level language and resembles assembly Language, the ANY_TO_TIME function converts the current result.
ST Language
Q := ANY_TO_TIME (IN);
FBD Language
FFLD Language
(* The conversion is executed only if EN is TRUE *)
(* ENO keeps the same value as EN *)
IL Language:
Op1: FFLD IN
ANY_TO_TIME
ST Q
See also
ANY_TO_BOOL ANY_TO_SINT ANY_TO_INT ANY_TO_DINT ANY_TO_LINT ANY_TO_REAL ANY_TO_LREAL ANY_TO_STRING