/   Divide

Operator - Performs a division of inputs.

Inputs

IN1 : ANY_NUM  First input
IN2 : ANY_NUM  Second input

Outputs

Q : ANY_NUM    Result: IN1 / IN2

Remarks

All inputs and the output must have the same type. In FFLD language, the input rung (EN) enables the operation, and the output rung keeps the same value as the input rung. In ILClosed"Instruction list" This is a low-level language and resembles assembly language, the DIV instruction performs a division between the current result and the operand. The current result and the operand must have the same type.

ST Language

Q := IN1 / IN2;

FBD Language

DivFbd.gif (1231 octets)

FFLD Language

(* The division is executed only if EN is TRUE *)
(* ENO is equal to EN *)
DivLd.gif (1485 octets)

IL Language:

Op1: FFLD  IN1
     DIV IN2
     ST  Q    (* Q is equal to: IN1 / IN2 *)
Op2: FFLD  IN1
     DIV IN2
     DIV IN3
     ST  Q    (* Q is equal to: IN1 / IN2 / IN3 *)

See also

+   -   *