AXIS#.CS.STATE
Description
AXIS#.CS.STATE returns the internal state machine value of the controlled stop.
0 = controlled stop is not occurring.
1 = controlled stop is occurring
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-00-00-000 |
|
General Information
Type |
Read Only |
Units |
N/A |
Range |
0 to 1 |
Default Value |
0 |
Data Type |
Integer |
Stored in Non Volatile Memory |
No |
Variants Supported
All variants are supported.
Fieldbus Information
Fieldbus![]() |
Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO![]() |
---|---|---|---|---|---|---|---|---|
EtherCAT![]() |
AXIS1.CS.STATE | 0x5002 | 0x1 | USINT | - | - | RO | False |
AXIS2.CS.STATE | 0x5102 | 0x1 | USINT | - | - | RO | False |