AXIS#.MOTOR.KT
Description
This parameter is the torque Torque is the tendency of a force to rotate an object about an axis. Just as a force is a push or a pull, a torque can be thought of as a twist constant of the motor.
-
- This parameter is automatically configured for Kollmorgen motors when MOTOR.AUTOSET=1.
Context
For more information see Motor.
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-00-00-000 |
General Information
Type |
Read/Write |
Units |
Nm/A |
Range |
0 to 1,000,000 |
Default Value |
0 |
Data Type |
Float |
See Also |
N/A |
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Fieldbus Information
Fieldbus![]() |
Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO![]() |
---|---|---|---|---|---|---|---|---|
EtherCAT![]() |
AXIS1.MOTOR.KT | 0x500B | 0x3 | UDINT | 1000:1 | - | RW | False |
AXIS2.MOTOR.KT | 0x510B | 0x3 | UDINT | 1000:1 | - | RW | False |