AXIS#.DISSOURCESMASK
Description
AXIS#.DISSOURCESMASK is a bit-field that returns all possible reasons why an axis could be disabled. If a bit is set, the drive can be disabled for this reason. The bits in this bit-field match AXIS#.DISSOURCES.
The return value specific bits are as follows:
Bit | Status and Response |
---|---|
0 | Software triggered disable |
1 | Fault exists |
2 | Hardware Enable input inactive |
3 | In-rush relay state prevents enable |
4 | Initialization not complete |
5 | Controlled stop requested from digital input |
6 | Field bus requested disable |
7 | Reserved |
8 | Reserved |
9 | STO disable (STO input is low) |
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-00-00-000 |
General Information
Type |
Read Only |
Units |
N/A |
Range |
N/A |
Default Value |
N/A |
Data Type |
Integer (bit-field) |
Stored in Non Volatile Memory |
No |
Variants Supported
All variants are supported
Fieldbus Information
Fieldbus![]() |
Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO![]() |
---|---|---|---|---|---|---|---|---|
EtherCAT![]() |
5000h | AXIS1.DISSOURCES | 8h | UINT | - | - | RO | False |
5100h | AXIS2.DISSOURCES | 8h | UINT | - | - | RO | False |