AXIS#.DISTO
Description
This timer starts when AXIS#.DIS is issued (regardless of the AXIS#.DIS origin). After this timeout elapses, the actual state of the drive is compared to the AXIS#.DISMODE setting. If the actual state does not match the AXIS#.DISMODE setting, a fault is reported and the hardware immediately executes the AXIS#.DISMODE setting (for instance, disable or activate dynamic brake). Setting AXIS#.DISTO to 0 will disable the timeout.
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-00-00-000 |
General Information
Type |
Read/Write |
Units |
ms |
Range |
0 to 120,000 ms |
Default Value |
1,000 ms |
Data Type |
Integer |
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported
Fieldbus Information
Fieldbus![]() |
Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO![]() |
---|---|---|---|---|---|---|---|---|
EtherCAT![]() |
AXIS1.DISTO | 0x5000 | 0x9 | UDINT | - | - | RW | False |
AXIS2.DISTO | 0x5100 | 0x9 | UDINT | - | - | RW | False |