AXIS#.STOP
Description
This command stops drive motion. In torque Torque is the tendency of a force to rotate an object about an axis. Just as a force is a push or a pull, a torque can be thought of as a twist and velocity modes, the command value will immediately be set to 0. In position mode, the axis will decelerate to a full stop. If the position command is from a gearing master, the drive will cancel gearing and decelerate to a stop. This command has no effect if the command source is an analog input.
If the command values are coming from a fieldbus master, the stop may be immediately overwritten by a new fieldbus command. Use a controlled stop input or disable command to ensure a stop.
The following table defines the behavior of AXIS#.STOP:
Cmdsource | Opmode | Subopmode | Deceleration ramp defined by: |
---|---|---|---|
Service | Torque![]() |
- | AXIS#.IL![]() |
Velocity | - | AXIS#.SM.DEC and AXIS#.SM.DEC | |
Position | Service motion | AXIS#.SM.DEC and AXIS#.SM.DEC | |
Motion tasking | AXIS#.MT.DEC | ||
Homing![]() |
AXIS#.HOME.DEC | ||
Fieldbus![]() |
Torque | - | Command has no effect. |
Velocity | |||
Position | |||
Electronic Gearing | Position | - | AXIS#.GEAR.DECMAX |
Analog | Torque | - | Command has no effect. |
Velocity | |||
Position |
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-00-00-000 | |
General Information
Type |
Command |
Units |
N/A |
Range |
N/A |
Default Value |
N/A |
Data Type |
N/A |
Stored in Non Volatile Memory |
No |
Variants Supported
All variants are supported
Fieldbus Information
Fieldbus | Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO![]() |
---|---|---|---|---|---|---|---|---|
EtherCAT![]() |
AXIS1.STOP | 0x5000 | 0xD | UDINT | - | - | wo | False |
AXIS2.STOP | 0x5100 | 0xD | UDINT | - | - | wo | False |