File Tools Function Blocks
This section documents function blocks that can be applied to files.
| Fucnction Block | Use |
|---|---|
| FileClose | Close an open file. |
| FileCopy | Copy a file. |
| FileDelete | Remove a file. |
| FileEOF | Test if the end of the file is reached in a file that is open for reading. |
| FileExists | Test if a file exists. |
| FileOpenA | Create or open a file in append mode. |
| FileOpenR | Open a file for reading. |
| FileOpenW | Create or reset a file and open it for writing. |
| FileReadBinData | Read binary data from a file. |
| FileReadLine | Read a string value from a text file. |
| FileRename | Rename a file. |
| FileSeek | Set the current position of a file. |
| FileSize | Get the size of a file. |
| FileWriteBinData | Write binary data to a file. |
| FileWriteLine | Write a string value to a text file. |