Motion Library - Sampler
-
-
See Pipe Block Descriptions for more information.
| Name | Description | Return type |
| MLSmpConECAT | Connects a sampler block to the specified CoE object in a PDO |
BOOL |
| MLSmpConnect | Connects a sampler block to a pipe network axis or pipe block. | BOOL |
| MLSmpConPLCAxis | Connects a sampler block to a PLCopen |
BOOL |
| MLSmpConPNAxis | Connects a sampler block to a Pipe Network axis variable. | BOOL |
| MLSmpInit | Initializes a sampler object. | BOOL |
-
-
There is a delay when using an external encoder.
The delay is five cycles:
2 cycles to read the encoder from the AKD via EtherCAT
***EtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs,
1 cycle for computing,
2 cycles for sending the new position set point to the AKD).
This lag error is speed proportional (5 cycles * speed).
A Phaser block can be used to compensate for this lag.