Error Handling Behavior
Two outputs deal with errors that can occur while executing a function block. These outputs are defined as follows:
- Error: The rising edge
A rising edge is the transition of a digital signal from low to high. It is also called positive edge of Error informs you that an error occurred during the execution of the function block. - ErrorID: Error number.
- See PLCopen Function Block ErrorID Output for more information.
- Done, InVelocity, InGear, and InSync mean successful completion.
- These signals are logically exclusive to Error.
- Instance errors do not always result in an axis error.
- Some bring the axis to StandStill.
- See Motion State Machine for more information.