Create a KVB Project
KVB projects are managed in the Project Explorer.
Use this procedure to create a project:
- In the Project Explorer, right-click on the System item to open the contextual menu.
- Select the Add HMI
"Human-machine interfaces "
Also known as computer-human interfaces (CHI), and formerly known as man-machine interfaces, they are usually employed to communicate with PLCs and other computers, such as entering and monitoring temperatures or pressures for further automated control or emergency response device command. - Select the device name within the list and click OK.
-
-
The content varies depending the version of KVB installed on your system.
If you have KVB 1.1 installed you may open projects that have a KVB 2.1 panel but you cannot open the panel in KVB. - Right-click on the newly created item and select the Rename command to change its name.
- Right-click and select the Add KVB Project command.
Figure 4-24: Select an AKI to add.
-
-
This command is disabled when a KVB panel is already created for the current HMI device.