Global Defines
Global Defines are user-generated constants used in a program.
Global Defines are used to write code and add an ifdef statement to call the Define only if it is used for a particular machine.
They are created and edited in the Project Explorer toolbox under PLC
"Programmable Logic Controller"
A Programmable Logic Controller, PLC, or Programmable Controller is a digital computer used for automation of industrial processes, such as control of machinery on factory assembly lines.
Used to synchronize the flow of inputs from (physical) sensors and events with the flow of outputs to actuators and events.
Double-click the Defines item to open the global definitions file (named: appli.eqv) in a text editor as:
Figure 4-95: Edit the Global Definitions
Each definition must be entered on one line of text using this syntax:
#define Identifier Equivalence (* comments *)
Definition Inside Another Definition
A definition within the contents of another definition is allowed.
The definition used in the second must be declared first.
Example:
#define PI 3.14
#define TWOPI (PI * 2.0)
Local Definitions
Local definitions are user-created defines used within the corresponding program through an ifdef statement.
-
-
Using definitions disturbs the program monitoring and makes error reports more complex.
It is recommended to restrict the use of definitions to simple expressions.
This helps avoid misunderstandings when reading or debugging a program.