Controller Log Files
- Logs generated on a PCMM or AKD PDMM are stored in flash memory at /mount/flash/log.
- Logs generated on a PCMM2G are stored in flash memory at /home/kas/kas/log.
Files are stored in a rotating pool consisting of a maximum of 10 files.
- The files have a maximum size of 200 kilobytes each.
- The most amount of space the log files will consume is 2MB.
- When a files is created after the tenth file, the earliest file is deleted to make room for the new file.
The controller-generated log levels can be controlled from the KAS IDE
"Integrated development environment"
An integrated development environment is a type of computer software that assists computer programmers in developing software.
IDEs normally consist of a source code editor, a compiler and/or interpreter, build-automation tools, and a debugger and Web Server. KAS IDE-generated log levels can be filtered in the configuration window in the Logs and Information tab.
Log File Naming Convention
The logs have this naming convention: pdmm_logs_n.
n is a value ranging from 0000000000 to 4294967295, which is the maximum value a 32-bit location can store.
Example
- When the files are first created they are named pdmm_logs_0000000000, pdmm_logs_0000000001, pdmm_logs_0000000002, etc.
- The file that is created after pdmm_logs_4294967295 is pdmm_logs_0000000000.
- The naming is reset and continues.