Display the IP Address of a Kollmorgen Controller
The IP Address assigned to the controller can be shown on the 7-segment display.
The IP may be displayed at boot and can be accessed from the Kollmorgen Controller's B3 Button Menu.
There is a 5 second delay before this function can be used again.
-
-
The PCMM, PCMM2G or AKD PDMM do not set (or show) an IP address without an attached network cable.