Web Server Home Page
To access the KAS web server home page, enter the controller's IP address.
This page provides an overview of the device including:
- Manufacturer
- CPU Speed
- CPU Cores
- Model Number
- Serial Number
- Hardware Revision
- TCP/IP MAC Address — a unique value associated with the TCP/IP network adapter that uniquely identifies the adapter on a LAN.
- EtherCAT
***EtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs MAC Address — a unique value associated with the EtherCAT network adapter that uniquely identifies the adapter on an EtherCAT network.
-
-
Any reference to AKD PDMM or PCMM refers to both the 800MHz and the single- and dual-core 1.2GHz variants, unless otherwise noted.