Log Data

KAS log files may be viewed from the Log Data tab. These messages can help describe the current state of the system and to help identify any operation errors encountered when developing your system. Controllers display as many as 10 files.

Figure 6-5: Example of Log Files from a Kollmorgen Controller's Webserver

Click a listed log file to open it in a web browser.

  • Click the green download icon next to the log entry to download the log file.
  • The default name is the same as the file's name.
  • If a file no longer exists, the message /logfiles/<selected file name> not found. appears.
    • Refresh the browser window and try again.

Figure 6-6: Example of a log file's content in a browser.


  • Controller log data is collected and updated every 15 seconds.
    A new log file is created when the current file is full.
    You may need to wait for up to 15 seconds for a log to show up in the list.
    The AKD PDMM and PCMM log files both have the same file naming scheme (pdmm_log_xxxxxxxxxx).

Log Message Content

Every log message in the table has this information:

Log Messages - List of Field

Field

Description

Time

Time when the log was recorded with the format:

DD-MMMM-YY hh:mm:ss (millisecond)

Source

Identifies a software or hardware component issuing the messages.

Each source is configured with a specific Level.

Level

Each message has one of these levels with importance in ascending order:

DEBUG > INFO > WARNING > ERROR > CRITICAL

Message

Text of the message issued from the source


  • Log messages are an important source of information when you are troubleshooting your project.
    When reporting an issue to Support, copy/paste the logs in the report.