Window Menu

Windows Menu Commands
Command Shortcut Description

MDI/Tabbed Workspace

ALT+W

Toggle the workspace between the MDIClosed "Multiple document interface" Graphical computer applications with an MDI are those whose windows reside under a single parent window (usually with the exception of modal windows), as opposed to all windows being separate from each other (single document interface). Advantages: - With MDI, a single menu bar and/or toolbar is shared between all child windows, reducing clutter and increasing efficient use of screen space - An application's child windows can be hidden/shown/minimized/maximized as a whole - Features such as "Tile" and "Cascade" can be implemented for the child windows and the tabbed mode

Cascade

ALT+C

Re-arrange all workspace children windows in cascade mode

Tile

ALT+T

Re-arrange all workspace children windows in tile mode

Reset IDE Layout Alt+R

This option resets widgets to their default location and visibility.

If an item is hidden or floating, it is made visible and returned to its default position.

These interface items are affected by this option: