Variables
All variables within the entire system project are grouped as follows:
|
Description |
|
|
Global variables |
List all global variables that are used and accessible throughout the entire program |
|
List all variables that are to be retained when the system is powered down |
|
|
Program variables |
List the variables related to your specific selected program |
For each variable, the Dictionary toolbox allows you to set the following parameters:
|
Description |
|
|
Name |
The variable name. |
|
Value |
All the variables in the Dictionary are animated with real-time values 1 Note that this column is only displayed when your application is running For more details, see "Variable Monitoring" |
|
Type |
The variable type (which can also be UDFB |
|
Dim. |
To declare an array, you can specify dimension(s) for an internal variable |
|
The variable attributes (Read Only, External, IN, OUT) as defined:
|
|
|
Init value |
The variable initial value when you start your application (see more details here) |
|
User Group |
The variable user group (used for sorting variables) |
|
Select variables to be used in HMI (see Map Variables to HMI) |
|
|
The variable tag is a short comment, that can be displayed together with the variable name in graphical editors. Edit the variable parameters Add the variable to your FBD Resize the rectangle to make the Tag and Description visible |
|
|
Description |
The variable description is a long comment text that describes the variable |
|
Syb. |
reserved |