AXIS#​.FIELDWEAKENING​.LOOPBW

Description

AXIS#.FIELDWEAKENING.LOOPBW determines the field-weakening-loop’s bandwidthClosed In computer networking, bandwidth often refers to a data rate measured in bits/s, for example, network throughput. The reason for the connection of data rate with the term bandwidth is that the limit to the data rate of a physical communication link is related to its bandwidth in hertz when entering the above-base-speed region.


  • The field weakening control loop is a nonlinear loop and the bandwidth increases as velocity increases. Always allow for 50% increase in the bandwidth.

To correctly set the internal parameters of the field weakening loop, based on the commanded bandwidth, the following motor parameters must be set correctly:

Versions

Action Version Notes
Implemented 02-06-00-000

 

General Information

Type

Read/Write

Units

Hz

Range

0 to 5000 Hz

Default Value

15 Hz

Data Type

Integer

Stored in Non Volatile Memory

Yes