AXIS#.MOTOR​.FIELDWEAKENING

Description

This parameter turns on field weakening control for rotary surface permanent magnet and interior permanent magnet motors (AXIS#.MOTOR.TYPE = 0 and 6). Field weakening allows a motor to operate above rated speed.

This keyword can only be set when AXIS#.MOTOR.TYPE = 0, 6, or 10. Any other AXIS#.MOTOR.TYPE results in an error and AXIS#.MOTOR.FIELDWEAKENING is not applied.

Context

For more information see Motor.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

N/A

Range

0 to 1

Default Value

0

Data Type

Integer

Stored in Non Volatile Memory

Yes

Variants Supported

All variants are supported.

Fieldbus Information

FieldbusClosed A Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design Parameter Index Sub-Index Data Type Float Scale Units Access PDOClosed PDO is a type of protocol frame used in some fieldbuses. A PDO contains one or more object dictionary entries, which define the application data transferred between devices. Mappable
EtherCATClosed ***EtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen AXIS1.MOTOR.FIELDWEAKENING 0x500B 0xF USINT - - RW False
AXIS2.MOTOR.FIELDWEAKENING 0x510B 0xF USINT - - RW False