AXIS#.MOTOR.INERTIA
Description
This parameter is the motor inertia. It is used to calculate the default velocity loop tuning gains (AXIS#.VL.KP ).
-
- This parameter is automatically configured for Kollmorgen motors when AXIS#.MOTOR.AUTOSET = 1 and can be modified while AXIS#.MOTOR.AUTOSET = 1 if its AXIS#.MOTOR.DISAUTOSET index = 1.
Context
For more information see Motor.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read/Write |
|
Units |
kgcm² for rotary motors |
|
Range |
0 to 200,000 |
|
Default Value |
0 |
|
Data Type |
Float |
|
See Also |
N/A |
|
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Fieldbus Information
| Fieldbus |
Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO |
|---|---|---|---|---|---|---|---|---|
| EtherCAT |
AXIS1.MOTOR.INERTIA | 0x500B | 0x11 | UDINT | 1000:1 | - | RW | False |
| AXIS2.MOTOR.INERTIA | 0x510B | 0x11 | UDINT | 1000:1 | - | RW | False |