AXIS#.MOTOR.PITCH
Description
This parameter is used with linear encoders. It defines a distance in millimeters which is determined by how the linear enocoder is used.
-
When used with a linear motor, it defines the pole-to-pole pitch. The pitch is the distance between two similar poles. Kollmorgen linear motors have a pitch of 32mm.
-
When using a linear encoder in a dual loop configuration in which the linear encoder is used as a secondary position feedback, the distance specified is equal to the distance the linear encoder travels given one rotation of the rotary motor.
-
-
This parameter is required to be configured for AXIS#.MOTOR.TYPE = 1 or when using a linear encoder as the AXIS#.PL.FBSOURCE.
Context
For more information see Motor.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 | |
| Added dual loop behavior | 02-09-03-000 | AXIS#.MOTOR.PITCH was not previously included in the resolution calculation when using a linear encoder only as a position source. In order to relate the rotary motor with the linear encoder for proper control, this parameter is now required to be set. |
General Information
|
Type |
Read/Write |
|
Units |
mm |
|
Range |
0.001 to 1000 |
|
Default Value |
32 |
|
Data Type |
Float |
|
See Also |
N/A |
|
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Fieldbus Information
| Fieldbus |
Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO |
|---|---|---|---|---|---|---|---|---|
| EtherCAT |
AXIS1.MOTOR.PITCH | 0x500B | 0x16 | UDINT | 1000:1 | - | RW | False |
| AXIS2.MOTOR.PITCH | 0x510B | 0x16 | UDINT | 1000:1 | - | RW | False |