AXIS#.MOTOR.TBRAKEAPP

Description

This parameter is the mechanical delay required for the motor brake to close. When disabling an axis using AXIS#.DISMODE not '0 - Disable axis immediately', the drive will servo to hold position for this time delay, allowing the brake to apply.


  • AXIS#.MOTOR.TBRAKEAPP has no effect when DISMODE is 0.

Context

For more information see Brake and Motor.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

ms

Range

0 to 1,000 ms

Default Value

75 ms

Data Type

Integer

See Also

N/A

Stored in Non Volatile Memory

Yes

Variants Supported

All variants are supported.

Fieldbus Information

FieldbusClosed A Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design Parameter Index Sub-Index Data Type Float Scale Units Access PDOClosed PDO is a type of protocol frame used in some fieldbuses. A PDO contains one or more object dictionary entries, which define the application data transferred between devices. Mappable
EtherCATClosed ***EtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen AXIS1.MOTOR.TBRAKEAPP 0x500B 0x1A UINT - - RW False
AXIS2.MOTOR.TBRAKEAPP 0x510B 0x1A UINT - - RW False