AXIS#.SETTLE.P
Description
Bits 11 and 15 of AXIS#.MOTIONSTAT use AXIS#.SETTLE.P to indicate that the target position of a motion task has been reached. AXIS#.MOTIONSTAT displays a "Target Position Reached" bit as soon as the following statement becomes true:
abs(actual_position – target_position) < AXIS#.SETTLE.P
Examples
Code
Sets the position window of motion task 0 to 10 degrees. The first parameter is the motion task number and the second is the position window value.
-->AXIS1.SETTLE.P 0 10 <<<note the removed 0>>>
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
This content is not applicable to KAS.
|
Type |
Read/Write |
|
Units |
Depends on AXIS#.UNIT.PROTARY Rotary: counts, rad, deg, Custom Units, 16-bit counts |
|
Range |
N/A |
|
Default Value |
180 [deg] |
|
Data Type |
Float |
|
See Also |
AXIS#.MOTIONSTAT |
|
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Fieldbus Information
| Fieldbus |
Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO |
|---|---|---|---|---|---|---|---|---|
| EtherCAT |
AXIS1.SETTLE.P | 0x5016 | 0x1 | UDINT | - | Position | RW | False |
| AXIS2.SETTLE.P | 0x5116 | 0x1 | UDINT | - | Position | RW | False |