EEO#.PIN

Description

EEO#.PIN is used in conjunction with EEO#.POUT to set the gain of the EEO position going to the EEO Generator. The maximum value of EEO#.PIN / EEO#.POUT is 32.

Versions

Action Version Notes
Implemented 02-07-00-000

General Information

Type Read/Write
Description Sets the gear IN of the EEO postision
Units N/A
Range 1 to 4,294,967,295
Default Value 1
Data Type Integer
See Also EEO#.POUT
Stored in Non Volatile Memory Yes

Variants Supported

All variants are supported.

Fieldbus Information

Fielldbus Parameter Index Sub-Index Data Type Float Scale Unitts Access PDOClosed PDO is a type of protocol frame used in some fieldbuses. A PDO contains one or more object dictionary entries, which define the application data transferred between devices. Mappable
EtherCATClosed ***EtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs and CANopen EEO1.PIN 0x4600 0x8 UDINT - - RW False
EEO2.PIN 0x4601 0x8 UDINT - - RW Falsi