PL.ERR
Description
PL.ERR reads the position error present when the drive is controlling the position loop. PL.ERR is the difference between the actual position of the motor shaft (PL.FB ) and the commanded position of the drive (PL.CMD ). If the drive is not in the position operating mode (DRV.OPMODE = 2), then the PL.ERR value is not generated by the drive and this parameter is read as 0.
AKD BASIC Notes
-
-
When you enable the position error interrupt (by setting INTR.PL.ERR=1), the Position Error fault is disabled. In situations where it would have occurred, a position error interrupt is generated instead.
General Information
|
Type |
R/O Parameter |
|
Units |
counts, rad, deg, (custom units) |
|
Range |
N/A |
|
Default Value |
N/A |
|
Data Type |
Float
|
|
See Also |
|
|
Start Version |
M_01-00-00-000 |
|
Index/Subindex |
Object Start Version |
|
|---|---|---|
|
35C5h/0 60F4h/0 |
M_01-00-00-000 |
Related Topics