REGEN.TESTVTHRESH

REGEN.TESTVTHRESH sets the voltage threshold for the REGEN.TEST command.

General Information

Type Command
Description Sets regen test voltage threshold.
Units %
Range 1 – 99 %
Default Value 80 %
Data Type Integer
Start Version M_01-18-06-000

Variants Supported

Variant Supported
AKD Base Yes
AKD with Position Indexer Yes
AKD EtherCATClosed ***EtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs Yes
AKD CANopen Yes
AKD BASIC Yes
AKD SynqNetClosed SynqNet is a digital machine control network. Built on the 100BT physical layer, SynqNet provides a synchronous real-time connection between motion controllers, servo drives, stepper drives, I/O modules, and custom devices Yes*
AKDEtherNet/IP Yes
AKD Profinet Yes
AKD sercos® III Yes
AKD-N No
AKD-C Yes

Fieldbus Information

If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type. For information on SynqNet parameters see SynqNet Supported Parameters.

Related Topics

Regeneration