List of Date / Time / NTP ErrorID Codes
- 23 = Internal error. See controller log for details.
- 15000 = Controller type does not support this function block.
- 16200 = Could not read NTP
"Network Time Protocol"
A networking protocol for clock synchronization between computer systems.
The PCMM2G can be configured to synchronize with public NTP time servers over the internet or a local NTP time server for networks that are not connected to the internet. server configuration file. - 16201 = Invalid time zone.
- 16202 = Cannot set date / time when NTP synchronization is active.
- 16203 = Invalid date / time value specified.