File Management
File Management functions provide the ability to:
- Read machine recipes or other machine operational data into the KAS program from the SD card, USB
"Universal Serial Bus"
USB is a serial bus standard to interface devices flash drive, or a shared directory. - Read cam tables into the program from the SD card, USB flash drive, or a shared directory.
- Store machine operational data in internal PxMM or PCMM2G flash memory (retrievable through the web server), the SD card, USB flash drive, or a shared directory.
-
A shared directory connection is setup through the web server.
-
-
- Functions to parse out information from a file using a string format can be found in String Operations.
- If the file is in a .CSV format, these functions can be used: LogFileCSV, ApplyRecipeColumn.
- You can create, store, and retrieve recipes and other data using either:
- the AKI Terminals. For more information see the KVB manual.
- an external bus connection to the PxMM or PCMM2G with a supported fieldbus (e.g., UDP or HTTP).
| Fucnction Block | Use |
|---|---|
| FileClose | Close an open file. |
| FileCopy | Copy a file. |
| FileDelete | Remove a file. |
| FileEOF | Test if the end of the file is reached in a file that is open for reading. |
| FileExists | Test if a file exists. |
| FileOpenA | Create or open a file in append mode. |
| FileOpenR | Open a file for reading. |
| FileOpenW | Create or reset a file and open it for writing. |
| FileReadBinData | Read binary data from a file. |
| FileReadLine | Read a string value from a text file. |
| FileRename | Rename a file. |
| FileSeek | Set the current position of a file. |
| FileSize | Get the size of a file. |
| FileWriteBinData | Write binary data to a file. |
| FileWriteLine | Write a string value to a text file. |
These functions handle mounting of SD cards:
| Name | Use |
|---|---|
| SD_ISREADY | Check that the SD card is ready for read/write |
| SD_MOUNT | Mount an SD card |
| SD_UNMOUNT | Unmount an SD card |
Each file is identified in the application by a unique handle manipulated as a DINT value.
- The file handles are allocated by the target system.
- Handles are returned by the Open function blocks and used by all other function blocks for identifying the file.
LogFileCSV log values of variables to a CSV file
-
-
- Opening a file with FileOpenA, FileOpenR, and FileOpenW can be unsuccessful (invalid path or file name, too many open files.)
- Your application must check the file ID for a NULL value.
- If the file ID is NULL (zero), then file read or write operations will fail.
- File management may be unavailable on some targets.
- Memory on the SD card is available in addition to the existing flash memory.
- Valid paths for storing files depend on the target implementation.
- Error messages are logged in the Controller log section of KAS Runtime
In computer science, runtime (or run-time) describes the operation of a computer program, the duration of its execution, from beginning to termination (compare compile time).
Within KAS, runtime also refers to the virtual machine that manage the program written in a computer language while it is running where there is a failure in any related function block. - Using the KAS Simulator, all path names are ignored, and files are stored in a reserved directory. Only the file name passed to the Open functions is taken into account.
- AKD PDMM / PCMM files are big endian.
- PCMM2G files are little endian.
- Opening a file with FileOpenA, FileOpenR, and FileOpenW can be unsuccessful (invalid path or file name, too many open files.)
-
- Review the File Path Conventions to understand hardware-based functional differences.