Hierarchy of SFC Programs
"Sequential function chart"
It can be used to program processes that can be split into steps.
The main components of SFC are:
- Steps with associated actions
- Transitions with associated logic conditions
- Directed links between steps and transitions program can have one or more child
programs.
- Child programs are written in SFC.
- They are started or stopped in the actions of the parent program.
- The number of hierarchy levels must not exceed 19.
- A child program can also have children.
- When a child program is stopped, its children are also stopped.
- When a child program is started, it must start its children.
- A child program is controlled (started or stopped) from the action blocks of its parent program.
- See Control an SFC Child Program for more information.
- Designing a child program is:
- a simple way to program an action block in SFC language.
- very useful for designing a complex process and separate operations due to different aspects of the process.
- Example: It is common to manage the execution modes in a parent program and to handle details of the process operations in child programs.