SFC Steps
- It is drawn as a square box in the SFC
"Sequential function chart"
It can be used to program processes that can be split into steps.
The main components of SFC are:
- Steps with associated actions
- Transitions with associated logic conditions
- Directed links between steps and transitions chart. - Each step of a program is identified with a unique number.
- At runtime
In computer science, runtime (or run-time) describes the operation of a computer program, the duration of its execution, from beginning to termination (compare compile time).
Within KAS, runtime also refers to the virtual machine that manage the program written in a computer language while it is running, a step can be either active or inactive according to the state of the program.
-
-
Select a step, transition, or jump and press Ctrl+ENTER to change its number.
All actions linked to the steps are executed according to the activity of the step.
| Inactive Step | Active Step |
|---|---|
In conditions and actions of the SFC program, you can test the step activity by specifying its name (GS plus the step number) followed by .X.
Example
|
GS100.X |
Is TRUE if step 100 is active. Expression has the BOOL data type. |
You can test the activity time of a step, by specifying the step name followed by .T.
- It is the time elapsed since the activation of the step.
- When the step is deactivated, this time remains unchanged.
- It will be reset to 0 on the next step activation.
Example
|
GS100.T |
Is the time elapsed since step 100 was activated. Expression has the TIME data type. |
Initial Steps
Initial steps represent the initial situation of the chart when the program is started.