Auto-completion of Words
"Structured text"
A high-level language that is block structured and syntactically resembles Pascal / IL
"Instruction list"
This is a low-level language and resembles assembly editor includes commands for automatic completion of typed words according to declared variables and data types.
Press Ctrl + Space or Ctrl + J to activate auto-completion.
- If you use auto-complete and there is no match for a variable name in the Dictionary, press ENTER to open the variable creation dialog box.
- Use the dialog box to define a new variable.

These features are available:
|
Auto-completion of: |
Action |
|---|---|
|
Variable Name |
|
|
FB Member |
Type the name of a function block instance (used either as an instance or a data structure). Press the point (.) after the name of the instance; a pop-up list opens with the names of possible members. |
Other Syntax-related Commands
When lines are selected, you can automatically indent them.
Press <Tab> or <Shift+Tab> to shift the lines to the left or right, by adding or removing blank characters on the left.