WAIT / WAIT_TIME
"Structured text"
A high-level language that is block structured and syntactically resembles Pascal program.
Syntax
WAIT<BOOL expression> ;WAIT_TIME<TIME expression> ;
Remarks
- The WAIT statement:
- Provides an easy way to program a state machine.
- This avoids the use of complex CASE structures.
- Verifies the attached Boolean expression and takes these actions:
- If the expression is TRUE, the program continues normally.
- If the expression is FALSE, then the execution of the program is suspended up to the next PLC
"Programmable Logic Controller"
A Programmable Logic Controller, PLC, or Programmable Controller is a digital computer used for automation of industrial processes, such as control of machinery on factory assembly lines.
Used to synchronize the flow of inputs from (physical) sensors and events with the flow of outputs to actuators and events cycle. The Boolean expression will be checked again during next cycles until it becomes TRUE. The execution of other programs is not affected.
- Provides an easy way to program a state machine.
- The WAIT_TIME statement suspends the execution of the program for the specified duration.
- The execution of other programs is not affected.
These instructions are available in ST language only and have no correspondence in other languages.
- The WAIT and WAIT_TIME instructions:
- Cannot be called in a User-Defined Function Block
A function block groups an algorithm and a set of private data. It has inputs and outputs. (UDFB
"User Defined Function Block"
UDFB can be used as a sub-function block in another program of the application. It is described using FBD, LD, ST or IL language. Input / output parameters of a UDFB (as well as private variables) are declared in the variable editor as local variables of the UDFB). - The use of WAIT or WAIT_TIME in a UDFB provokes a compile error.
- Can be called in a sub-program.
- However, it can lead to some unsafe situation if the same sub program is called from various programs.
- Do not support re-entrancy.
- Avoiding this situation is the responsibility of the programmer.
- The compiler outputs some warning messages if a sub-program containing a WAIT or WAIT_TIME instruction is called from more than one program.
- Must not be called from ST parts of SFC
"Sequential function chart"
It can be used to program processes that can be split into steps.
The main components of SFC are:
- Steps with associated actions
- Transitions with associated logic conditions
- Directed links between steps and transitions programs. - This makes no sense as SFC is already a state machine.
- The use of WAIT or WAIT_TME in SFC or in a sub-program called from SFC provokes a compile error.
- Are not available when the code is compiled through a "C" compiler.
- Using "C" code generation with a program containing a WAIT or WAIT_TIME instruction provokes an error during post-compiling.
- Cannot be called in a User-Defined Function Block
- This statement is an extension to the standard and is NOT IEC
"International Electrotechnical Commission"
IEC is a not-for-profit, non-governmental international standards organization that prepares and publishes International Standards for all electrical, electronic and related technologies 61131-3 compliant.
-
-
This instruction is NOT UDFB safe.
Do not use inside UDFBs.
FBD Language
Not available.
FFLD Language
Not available.
IL Language
Not available.
ST Language
(* use of WAIT with different kinds of BOOL expressions *)
WAIT BoolVariable;
WAIT (diLevel > 100) AND NOT bAlarm;
WAIT SubProgCall ();
(* use of WAIT_TIME with different kinds of TIME expressions *)
WAIT_TIME t#2s;
WAIT_TIME TimeVariable;