DriveParamRead

PLCopen motion icon Pipe Network motion icon

 Function Block - Reads a drive parameter by sending an ASCII command to a drive.

Inputs

Input

Data Type

Range

Unit

Default

Description

Execute

BOOL

FALSE, TRUE

N/A

No default

On the rising edge of Execute, a drive parameter is read.

  • The function block processes only one request at a time.
  • If Execute is toggled quickly so that another rising edge occurs before the function block has completed, the function block does not issue a second read command.

Drive

INT

-32768 to +32767

N/A

No default

The address of the drive where data is read.

  • The first node usually has the value 1001.
  • The second node usually has the value 1002.

  • Use the members of the EtherCAT structure to specify a device's address to Create Variables.
       

Param

STRING

No range

N/A

No default

The parameter to read.

Outputs

Output

Data Type

Range

Unit

Description

Done

BOOL

FALSE, TRUE

N/A

Indicates whether this function block has completed without error.

Error

BOOL

FALSE, TRUE

N/A

Indicates whether this function block has completed with error.

ErrorID

DINT

No range

N/A

The DriveParamRead error result if Error is TRUE.

  • See Error Codes.
  • Upon success, Error is set to 0 (zero).

Value

LREAL

No range

N/A

The value of the drive parameter.

Value is only set when the function block has successfully completed.

Units

STRING

No range

N/A

The value of the drive parameter.

Value is only set when the function block has successfully completed.

Remarks

Notes

  • This function block uses and reserves the EtherCAT SDO Channel.
  • The SDO Channel remains reserved until the done output is TRUE.
  • This FB should be called at each cycle until either the Done or Error output is TRUE.
    • If it is not called at each cycle, the rest of SDO communication (e.g., the AKD GUI Views) is blocked.
  • Using this FB in SFC P0 or P1 steps is not recommended because these steps are executed only once.
  • If this FB is used in P0 or P1, then it must be used in an SFC N step to ensure the FB completes.

Usage

Use this function block to read drive parameters that are not supported by other function blocks.

Examples include:

  • Drive bus voltage
  • Drive display
  • Fault history
  • Motor temperature
  • Present drive limit settings
  • Present regeneration loading
  • It takes multiple cycles to complete this function block.
  • Typically only one DriveParamRead or DriveParamWrite function should be active for each axis at one time.
  • If executing this function block continuously or if multiple times is required, add code that waits for this function block to complete (e.g., Done bit = 1) before executing it again.
  • See EtherCAT Function Blocks that Work with Drive Parameters about function blocks not supported by ML and MC function blocks.

Figure 1: DriveParamRead

Error Codes

FBD Language Example

FFLD Language Example

IL Language Example

Not available.

ST Language Example

(* Read PL.KP on first AKD Drive on EtherCAT network *)
      
(* The code continually calls the FB (without re-executing it) until the first execution is done, then reads the returned value from the drive and reset the FB *)

IF ReadPropGain then
Inst_DriveParamRead1( 1, 1001, 'PL.KP' );
End_If;

On Inst_DriveParamRead1.Done do
Inst_DriveParamRead1( 0, 1001, 'PL.KP' );
PositionProportionalGain := Inst_DriveParamRead1.Value; (* Reads the returned value from the drive *)
ReadPropGain := 0; (* Reset the FB *)
End_DO;

See Also

DriveParamWrite