MC_GrpReadCmdVel
Function Block - Reads the command velocity of the axes in the group and the path velocity.
Inputs
|
Input |
Data Type |
Range |
Unit |
Default |
Description |
||||||||
|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
|
Enable |
BOOL |
FALSE, TRUE |
N/A |
No default |
If TRUE, this function block reads the current commanded velocity of the group and the axes in the group. |
||||||||
|
AxesGroup |
No range |
N/A |
No default |
The axes group the commanded velocity is read from. |
|||||||||
|
CoordSystem |
SINT |
Enumerated |
N/A |
No default |
|
||||||||
|
Velocity |
LREAL[ ] |
Dimension: The number of axes mapped in the AxesGroup. No range |
User unit/sec |
No default |
An array where the velocity data is written.
|
Outputs
|
Output |
Data Type |
Range |
Unit |
Description |
|---|---|---|---|---|
|
Valid |
BOOL |
FALSE, TRUE |
N/A |
If TRUE, the velocities were read without error. |
|
Error |
BOOL |
FALSE, TRUE |
N/A |
If TRUE, an error has occurred. |
|
ErrorID |
INT |
Enumerated |
N/A |
|
|
PathVelocity |
LREAL |
No range |
User unit/sec |
|
Remarks
-
-
This function or function block returns cached data.
See Program a Multi-Core Controller.
- See Coordinated Motion, the top-level topic for Coordinated Motion.
- See Function Blocks - General Rules about how inputs and outputs work.
- The MC_GrpReadCmdVel function block fills the array specified by the
Velocityargument with the commanded velocity for the coordinate system, which is specified by theCoordSystemargument.- The path velocity is reported by the PathVelocity output.
- This function or function block does not generate any motion.
-
-
Only the ACS coordinate system is supported.
See Coordinate Systems.
- There is a one-to-one correspondence between the axes in the Axes Group and the velocity values in the Velocity Array.
- If a index in the Axes Group is unassigned, the velocity value for that array element in the Velocity array is 0 (zero).
- If the element does contain an axis, the velocity value is filled with the current actual velocity for that axis.
Figure 1: MC_GrpReadCmdVel
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
(*MC_GrpReadCmdVel ST example *)
Inst_MC_GrpReadCmdVel(DoRead, Group, CoordSys, VelList );
See Also