MC_ErrorDescription

PLCopen motion icon Pipe Network motion icon

 Function - Converts the PLCopen error IDs into message strings.

Inputs

Input

Data Type

Range

Unit

Default

Description

En

BOOL

FALSE, TRUE

N/A

No default

If TRUE, this function converts the ErrorID to a string message.

ErrorID

INT

0 to 69

N/A

No default

Outputs

Output

Data Type

Range

Unit

Description

OK

BOOL

FALSE, TRUE

N/A

If TRUE, the command completed successfully.

Description

STRING

No range

N/A

String error description.

Remarks

  • Return a text description corresponding to a motion control error ID code.
  • The message strings can be used for display or logging.

Figure 1: MC_ErrorDescription

FBD Language Example

FFLD Language Example

IL Language Example

Not available.

ST Language Example

Description:= MC_ErrorDescription(ErrorID);