MLMotionCycleTime
Function - Returns the Motion Base Cycle time in seconds.
Inputs
|
Input |
Data Type |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
Enable |
BOOL |
FALSE, TRUE |
N/A |
No default |
Enable execution of the function. |
Outputs
|
Output |
Data Type |
Range |
Unit |
Description |
|---|---|---|---|---|
|
OK |
BOOL |
FALSE, TRUE |
N/A |
If TRUE, the command completed successfully. |
|
CycleTime |
LREAL |
0.00025 to 0.004 |
Seconds |
PLC cycle period in seconds. |
Remarks
None
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
//Read EtherCAT cycle rate in seconds
CycleTime := MLMotionCycleTime();