MC_CreatePLCAxis
Function - Creates a PLCopen Axis.
Inputs
|
Input |
Data Type |
Range |
Unit |
Default |
Description |
||||||||||||
|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
|
En |
BOOL |
FALSE, TRUE |
N/A |
No default |
When TRUE, requests to create a PLCopen axis. |
||||||||||||
|
AxisName |
STRING |
No range |
N/A |
No default |
Axis name. |
||||||||||||
|
BusInterface |
STRING |
No range |
N/A |
No default |
Bus interface identifier:
|
||||||||||||
|
BusAddress |
DINT |
Bus dependent |
N/A |
No default |
Address of the drive on the bus. |
||||||||||||
|
AxisNumber |
UINT |
1 to 256 |
N/A |
No default |
Axis number. |
||||||||||||
|
AxisType |
USINT |
Enumerated |
N/A |
No default |
One of these enumeration values:
|
||||||||||||
|
DriveAxisNumber |
UINT |
1 to 256 |
N/A |
No default |
This one-based number specifies the axis on the drive. For a single-axis drive this number should be 1. |
||||||||||||
|
UserUnits |
DINT |
1 to 2147483647 |
User units |
No default |
User unit portion of the user unit/feedback unit ratio. |
||||||||||||
|
FeedbackUnits |
DINT |
1 to 2147483647 |
Feedback units |
No default |
Feedback unit portion of the user unit/feedback unit ratio. |
||||||||||||
|
Rollover |
LREAL |
0 to 4294967296 |
User units |
No default |
Rollover position. 0 (zero) = no rollover. |
||||||||||||
|
UpdateRate |
UINT |
3 to 9 |
N/A |
No default |
Servo update rate.
|
Outputs
|
Output |
Data Type |
Range |
Unit |
Description |
|---|---|---|---|---|
|
OK |
BOOL |
FALSE, TRUE |
N/A |
Indicates the axis has been created. |
Figure 1: MC_CreatePLCAxis
Remarks
- See Function Blocks - General Rules about how inputs and outputs work.
- A call to this function is automatically generated when the application is compiled, based on the data entered in the PLCopen Axis Data dialog.
- MC_CreateAxis must be called between MLMotionInit and MLMotionStart.
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
(* MC_CreatePLCAxis ST Example *)
AxisName1 := 'PLCOpenAxis1';
BusName1 := 'EtherCATDriver';
BusAddress1 := 1001;
AxisNumber1 := 1;
AxisType1 := MC_AXIS_TYPE_SERVO_STEPPER;
DriveAxisNumber1 := 1;
UserUnits1 := 360;
FeedbackUnits1 := 1048576;
Rollover1 := 0;
UpdateRate1 := 3;
MC_CreateAxis(AxisName1, BusName1, BusAddress1, AxisNumber1, AxisType1, DriveAxisNumber1, UserUnits1, FeedbackUnits1, Rollover1, UpdateRate1);