MLAddWriteInput

Pipe Network motion icon

 Function - Sets the source of an input of an Adder Pipe Block.

Inputs

Input

Data Type

Range

Unit

Default

Description

BlockID

DINT

1 to 1024

N/A

No default

ID number of an initiated Adder object.

InputID

DINT

1 to 2

N/A

No default

Select first or second input to the Adder object.

InputBlockID

DINT

1 to 1024

N/A

No default

  • ID number of an initiated Pipe Block.
  • This is an input to the Adder object.

Outputs

Adder Block Output = Ratio1*Input1 + Offset1 + Ratio2*Input2 + Offset2

Output

Data Type

Range

Unit

Description

Default (.Q)

BOOL

FALSE, TRUE

N/A

Remarks

  • Function block is automatically called if an Adder Block is connected to other blocks in the Pipe Network.

Figure 1: MLAddWriteInput


  • Adder objects are normally created in the Pipe Network using the graphical engine.
    You do not have to add MLAddWriteInput function blocks to their programs.
    Blocks are connected with lines in the Pipe Network.
    The code is automatically added to the current project.

FBD Language Example

FFLD Language Example

IL Language Example

Not available.

ST Language Example

//Set the first input of an Adder pipeblock to be connected to the output of GEAR1 pipeblock
MLAddWriteInput( PipeNetwork.ADDER, 1, PipeNetwork.GEAR1 );

See Also