MLAxisGenIsRdy

Pipe Network motion icon

 Function - Verifies if an axis is ready.

Specifies whether the Axis generator is ready.

Inputs

Input

Data Type

Range

Unit

Default

Description

ID

DINT

1 to 1024

N/A

No default

ID of the Axis block.

Outputs

Output

Data Type

Range

Unit

Description

Default (.Q)

BOOL

FALSE, TRUE

N/A

Remarks

FBD Language Example

FFLD Language Example

IL Language Example

Not available.

ST Language Example

 MLAxisGenIsRdy(PipeNetwork.Axis1 );

See Also