MLAxisIsTrigged
Function - Verifies if the axis received a trigger event.
Inputs
|
Input |
Data Type |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
ID |
DINT |
1 to 1024 |
N/A |
No default |
ID of the Axis block. |
|
InputID |
DINT |
See Description. |
N/A |
No default |
ID of the triggered Fast input of an axis (i.e., IN1 and IN2 on S300). InputID INT Range = 0 to 1
|
|
edge |
DINT |
See Description. |
N/A |
No default |
Configures the Inputs as:
|
Outputs
|
Output |
Data Type |
Range |
Unit |
Description |
|---|---|---|---|---|
|
Default (.Q) |
BOOL |
FALSE, TRUE |
N/A |
|
Remarks
Returns TRUE if the Fast Input event has been triggered and not yet been reset.
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
MLAxisIsTrigged (PipeNetwork.Axis1, 0,1 ) ;
See Also